15.3.4.4 Center to Net Driver

This feature allows you to easily retrieve the driver of a net.

To go to the net driver:

  1. Select a net in NetlistViewer.
  2. From either the Schematic menu or right-click menu, choose Go to Net Driver.

    NetlistViewer displays the actual driver of the net. For example, in the sample design shown below, U1374 is a hierarchical block. Selecting the net connected to its output pin, and then choosing Go to Net Driver from the right-click menu displays instance U19 inside of block U1374 because instance U1374/U19 is the actual driver of the net.

Figure 15-21. Go to Net Driver
???
Figure 15-22. Zooms to and Selects Actual Driver of the Net (U19)
???
Note: When you choose Go to Net Driver, NetlistViewer selects the driver of the net to help you find it easily.