13.16.2 VBOOT Voltage Regulator
The VBOOT voltage regulator rail is used to supply bias voltage for the integrated 3-phase power MOSFET bridge drivers.
The regulator is capable of supplying 30 mA of external load current. The regulator has a minimum overcurrent limit of 40 mA.
The regulator gets its power from the integrated charge pump. When operating at supply voltages (HVDD) that are above +13.5V, the integrated charge pump will be disabled and the HVDD supply will power the VBOOT voltage regulator. The VBOOT regulator output may be lower than the designed voltage, while operating in the HVDD range of +12.5V to +13.0V, due to the dropout voltage of the regulator.
The VBOOT regulator requires an output capacitor, connected from VBOOT to LIN_VSS, to stabilize the internal control loop and to sustain the bootstrap capacitor energy. A minimum of 4.7 µF ceramic output capacitance is required for the VBOOT voltage regulator output; 10 µF is recommended when switching large MOSFET gate loads. The output capacitor forces a time delay between setting the OE pin high (to transition from Standby mode to Active mode) and the VBOOT regulator voltage output rising above the voltage required to set an internal VBOOT ready flag. The PWM inputs must not be activated while the VBOOT output is charging the output capacitors to the VBOOT ready voltage (typically 6.0V). The time required before allowing the PWM inputs to become active, after setting OE high to transition from Standby mode to Active mode, is dependent on output capacitance, any extra loads and supply voltage ramp-up time. The user should allow a minimum time of 0.94 ms for the VBOOT output voltage to rise above the VBOOT ready voltage. A voltage of 6V and supply current of 30 mA may be used for this delay estimation. See Equation 13-2.
There is a time-out function that allows the state machine to move from VBOOT to active after 15 ms, regardless of the VBOOT ready voltage. This time-out function prevents the driver from hanging up if the VBOOT voltage is overloaded.
There is also a capacitive voltage divider formed by the three bootstrap capacitors and the VBOOT capacitor. The VBOOT capacitor should be selected so that when the VBOOT supply is active and the bootstrap capacitors are charged, the voltage at the bootstrap capacitors will be greater than the driver undervoltage shutdown voltage, 4.5V. For a system with VBOOT = 12V, VMIN = 4.5V and N = 3 x 1 µF CBOOTSTRAP capacitors charging at the same time, the desired CVBOOT capacitor is 1.8 µF (see Equation 13-3). Since the VBOOT supply requires a 4.7 µF capacitor, a 4.7 µF capacitor should be used. The initial voltage seen by the bootstrap capacitors using a 4.7 µF VBOOT capacitor will be 7.32V. See Equation 13-4.
The VBOOT output is disabled when the driver transitions to Standby or Sleep mode. Table 13-5 shows the Faults that will also disable the VBOOT voltage regulator.