1.8.7.2 SmartBERT
(Ask a Question)SmartBERT enables you to run diagnostic tests on the transceiver lanes. SmartBERT uses the PRBS generator and checker functionality available in each transceiver lane to determine a lane's bit error rate (BER). The various PRBS patterns supported are PRBS7(SmartBERT IP), PRBS9(SmartBERT IP), PRBS15(SmartBERT IP), PRBS23(SmartBERT IP), and PRBS31(SmartBERT IP). Near-end loopback can be performed using one of these PRBS patterns.
To run SmartBERT in Debug TRANSCEIVER, follow these steps:
- Select the SmartBERT tab in the Debug TRANSCEIVER window.
- Select LANE in the left pane.
- Select the Pattern from the drop-down list.
- Select the EQ-NearEnd check box to enable internal loop-back, (this step can be ignored if external loop-back is enabled).
- Click Start. This
enables both transmitter and the receiver for a particular lane and for a particular
PRBS pattern. The following figure shows the Debug TRANSCEIVER window and the PRBS
pattern options for SmartBERT.
Figure 1-39. Debug TRANSCEIVER—Smart BERT When a SmartBERT IP lane is added, the Error Injection column is displayed in the right pane. The error injection feature is provided to inject an error while running a PRBS pattern. This feature is unavailable if regular lanes are added. Also, this feature is enabled only for SmartBERT IP supported PRBS patterns.
- Select Reset to clear the error count under Cumulative Error Counter. Error Count is displayed when the lane is added.
Figure 1-39 shows the Smart BERT tab and status of the TXPLL, RXPLL, Lock to Data, Data rate, and the BER.