1.8.7.9 Optimize Receiver

SmartDebug uses the Receiver coefficients to optimize the settings for the overall signal integrity at the receiver.

To run Optimize Receiver, perform the following steps:

  1. In Debug Transceiver, go to Signal Integrity and click on Optimize Receiver.
  2. In Optimize Receiver window the following settings
    • Select Lanes to Optimize Receiver: Lane0
  3. Click Optimize Receiver on selected Lanes.

Software based Optimizing Receiver process is successful on all selected lanes.

Figure 1-49. Optimize Receiver