1.1.3.4.2 DRV_METROLOGY_Reinitialize Function
C
SYS_MODULE_OBJ DRV_METROLOGY_Reinitialize (
SYS_MODULE_INIT * init
);Summary
Re-initializes the metrology driver according to the init parameter.
Description
This routine re-initializes the metrology driver resetting the Core 1 and re-loading the metrology library application on Core 1 from the scratch. The initialization data is specified by the init parameter. It is a single instance driver.
Precondition:
The low-level board initialization must have been completed and the module's initialization function must have been called before the system.
Parameters
| Param | Description |
|---|---|
| init | Pointer to the init data structure containing any data necessary to initialize the driver. |
Returns
If successful, returns a valid handle to a driver instance object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.
Example
SYS_MODULE_OBJ sysObjDrvMet;
extern uint8_t met_bin_start;
extern uint8_t met_bin_end;
/* Metrology Driver Initialization Data */
DRV_METROLOGY_INIT drvMetrologyInitData = {
/* MET bin destination address */
.regBaseAddress = DRV_METROLOGY_REG_BASE_ADDRESS,
/* MET Binary start address */
.binStartAddress = (uint32_t)&met_bin_start,
/* MET Binary end address */
.binEndAddress = (uint32_t)&met_bin_end,
};
sysObjDrvMet = DRV_METROLOGY_Initialize((SYS_MODULE_INIT *)&drvMetrologyInitData);Remarks
This routine must be called before any other DRV_METROLOGY routine is called.