1.1.3.4.17 DRV_METROLOGY_GetEnergyValue Function
C
uint32_t DRV_METROLOGY_GetEnergyValue(bool restartEnergy);Summary
Gets the active energy value.
Description
Gets the active energy value.
Parameters
| Param | Description |
|---|---|
| restartEnergy | Flag to indicate if the energy value should be restarted or accumulated to the previous calculated value. |
Returns
The active energy value obtained according to the last call to DRV_METROLOGY_UpdateMeasurements() routine.
Example
/* Send new Energy values to the Energy Task */
app_metrologyData.queueFree = uxQueueSpacesAvailable(appEnergyQueueID);
if (app_metrologyData.queueFree)
{
newMetrologyData.energy = DRV_METROLOGY_GetEnergyValue(true);
newMetrologyData.Pt = DRV_METROLOGY_GetRMSValue(RMS_PT);
xQueueSend(appEnergyQueueID, &newMetrologyData, (TickType_t) 0);
}
else
{
SYS_CMD_MESSAGE("ENERGY Queue is FULL!!!\n\r");
}Remarks
None.