1.1.3.4.29 DRV_METROLOGY_CALIBRATION_CALLBACK Typedef
C
typedef void (* DRV_METROLOGY_CALIBRATION_CALLBACK)(bool result);
Summary
Defines the data type and function signature for the callback function of the calibration procedure.
Description
The Metrology driver will call back the client's function with this signature when the Calibration procedure has been completed.
Parameters
| Param | Description |
|---|---|
| result | Flag o indicate if at least one phase has been calibrated successfully. Otherwise none of the phases have been calibrated. |
Returns
None.
Remarks
None.