21.13.1.81 xcvr_import_register
(Ask a Question)Description
This Tcl command imports exported transceiver registers details from a *.csv
file.
xcvr_import_register \
-file_name {absolute or relative path to the *.csv file name}
Arguments
Parameter | Type | Description |
---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
file_name | string | Path of the exported transceiver file. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'file_name' is missing. |
None | Parameter 'file_name' has illegal value. |
None | Register Access: file specified for Import must have .csv extension. |
None | Register Access: Must specify '-file_name. |
None | Parameter 'param_name' is not defined. Valid command formatting is'xcvr_import_register -file_name "File Name"'. |
Supported Families
PolarFire |
PolarFire SoC |
Example
Import previously exported transceiver registers details from a .csv file:
xcvr_import_register -file_name {register_list.csv}