21.13.1.62 set_debug_device

Description

Sets the device name in the tool.

set_debug_device -name “device name”

Arguments

ParameterTypeDescription

name

string

Specify the name of the device. This argument is mandatory.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None​

Parameter 'param_name' is not defined. Valid command formatting is 'set_debug_device -name "device name"

None​

Required parameter 'name' is missing.

Supported Families

PolarFire
PolarFire SoC
SmartFusion 2
IGLOO 2
RTG4

Example

The following example sets MPF250T_ES as the device name:

set_debug_device -name “MPF250T_ES”