21.13.1.30 mss_export_register
(Ask a Question)Description
This command reads the selected registers by mss_add_register command and save the content to a *.csv
file.
mss_export_register -file_name {path the file} [-all]
Arguments
Parameter | Type | Description |
---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
file_name | string | Specifies the path to the file, where the command saves the exported data. |
all | none | This is an optional parameter that is used to export all registers shown in the hierarchy. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Register Access: Must specify '-file_name. |
None | Parameter 'file_name' has illegal value. |
None | Register Access: file specified for Export must have .csv extension. |
None | Cannot export register information to the file: List of selected registers is empty. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'mss_export_register [-deviceName "device name"] [-file_name "File Name"] [-all "TRUE | FALSE"]'. |
Supported Families
PolarFire SoC |
Example
This example exports all mss registers into {./mss_exp.csv} file.
mss_export_register -file_name {./mss_exp.csv} -all
See Also
mss_add_register
mss_read_register
mss_write_register