21.13.1.80 xcvr_export_register
(Ask a Question)Description
This Tcl command exports previously added transceiver registers details to a *.csv file.
xcvr_export_register [-deviceName {device name}] \
[-file_name {file Name}] [-all]
Arguments
Parameter | Type | Description |
---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the |
file_name | string | Path of the export file. |
all | none | Specify to export all transceiver registers details to *.csv file. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'param_name' is not defined. Valid command formatting is'xcvr_export_register [-deviceName "device name"] [-file_name "File Name"] [-all "TRUE | FALSE"]'. |
None | Parameter 'file_name' has illegal value. |
None | Register Access: file specified for Export must have .csv extension. |
None | Register Access: Must specify '-file_name. |
Supported Families
PolarFire |
PolarFire SoC |
Example
Export previously added transceiver registers details to a .csv file:
xcvr_export_register -file_name {register_export.csv}
See Also
xcvr_add_register
xcvr_read_register
xcvr_write_register