21.13.1.20 import_ddc_file

Description

This is a Standalone SmartDebug command. Enables you to import DDC file (created through Export SmartDebug Data in Libero) into the debug project.

import_ddc_file -import_ddc "DDC file" -device_name "device name"

Arguments

ParameterTypeDescription

import_ddc

string

Specify path to the DDC file. This parameter is mandatory.

device_name

string

Specify the device name. This parameter is mandatory.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Required parameter 'import_ddc' is missing.

None

Required parameter 'device_name' is missing.

None

Failed to import DDC file '*.ddc'. There is no device 'device_name' in the current JTAG chain.

None

Parameter 'param_name' is not defined. Valid command formatting is

'import_ddc_file -import_ddc "DDC file" -device_name "device name"'

Supported Families

PolarFire
SmartFusion 2
IGLOO 2
RTG4

Example

This example importes DDC file to the debug project:

import_ddc_file -import_ddc {./src/top.ddc} -device_name {MPF250T_ES}

See Also

  • new_project