21.13.1.13 eye_monitor_power

Description

This tcl command switches on and off power eye monitor.

eye_monitor_power [-deviceName "device name"] \
                  -switch {on | off} \
                  -lane {physical lane name}

Arguments

ParameterTypeDescription

deviceName

string​

Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command.

switch

string

This argument specifies if the eye monitor is on or off.

lane

string

Specify the physical lane instance name.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Eye Monitor Power On/Off: Lane name not found in the list of assigned physical lanes in Libero.Provide the correct lane name.

None

Parameter 'lane' has illegal value.

None

Parameter 'switch' has illegal value.

None

Parameter 'param_name' is not defined. Valid command formatting is'eye_monitor_power [-deviceName "device name"] [-switch "Eye Monitor Power"] [-lane "Physical Lane Name"]'.

Supported Families

PolarFire
PolarFire SoC

Example

This example turns on the eye monitor.

eye_monitor_power -switch {on} -lane {Q0_LANE0}

This example turns off the eye monitor.

eye_monitor_power -switch {off} -lane {Q0_LANE0}