21.13.1.64 set_hsm_params
(Ask a Question)Description
Saves HSM parameters for the SmartDebug application. These parameters remain in effect until overridden by another invocation of this command.
set_hsm_params -hsm_server_name "hsm_server"
Arguments
Parameter | Type | Description |
---|---|---|
-hsm_server_name | string | Specifies the name or IP address of the HSM server computer. |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'hsm_server_name' is missing. |
None | Could not get server information. Check server address and connection and try again. |
None | HSM server name cannot be empty. |
None | hsm_type_u: Invalid argument value: '' (expecting TRUE, 1, true, FALSE, 0 or false). |
None | Warning:Deprecated 'hsm_type_u' parameter is used. |
None | FTP login password must be specified along with the user name. |
Supported Families
PolarFire |
SmartFusion 2 |
IGLOO 2 |
Example
This example sets the IP address of the server name computer.
set_hsm_params - hsm_server_name {10.241.140.224}