21.13.1.59 serdes_lane_reset

Description

This Tcl command resets lane in EPCS and PCI Lane modes. The result is shown in the log window/console.

serdes_lane_reset -serdes "integer value" -lane "integer value"

Arguments

ParameterTypeDescription

deviceName

string

Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command.

serdes

integer

Specifies SerDes block number. It must be between 0 and 4 varies between dies. It must be one of the SerDes blocks used in the design.

lane

integer

Specifies SerDes lane number. It must be between 0 and 3. It must be one of the lanes enabled for the block in the design.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Required parameter 'serdes' is missing.

None

Parameter 'serdes' has illegal value.

None

Required parameter 'lane' is missing.

None

Parameter 'lane' has illegal value.

None

Parameter 'param_name' is not defined. Valid command formatting is 'serdes_lane_reset [-deviceName "device name"] -serdes "integer value" -lane "integer value"'.

Supported Families

SmartFusion 2
IGLOO 2
RTG4

Example

This exmaple resets Lane 0, for specified SerDes block:

serdes_lane_reset -serdes 0 -lane 0

See Also

  • serdes_read_regster

  • serdes_write_regster