21.13.1.79 xcvr_add_register
(Ask a Question)Description
This Tcl command adds transceiver registers details to the SmartDebug register access interface.
xcvr_add_register [-deviceName {device name} \
[-reg_name {Add Register Names}]
Arguments
Parameter | Type | Description |
---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required, if there is only one device in the current configuration, or a device has already been selected using the |
reg_name | string | Name of the register. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | reg_name register is not added to Register access list. |
None | Parameter 'reg_name' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'xcvr_add_register [-deviceName "device name"] [-reg_name "Add Register Names"]'. |
None | Register Access: Must specify '-reg_name |
Supported Families
PolarFire |
PolarFire SoC |
Example
This example adds all the registers under the {SERDES1} component.
xcvr_add_register -reg_name {SERDES1}
See Also
xcvr_export_register
xcvr_read_register
xcvr_write_register