21.13.1.37 plot_eye

Description

This Tcl command is used to plot eye and export eye plots.

plot_eye [-deviceName "device name"] \
         -lane "Physical Lane Name" \
         [-file "filename"]

Arguments

ParameterTypeDescription

deviceName

string

Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command.

lane

string

Specify the lane instance name.

file

string

Specify the path to the location where the file is to be exported.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Required parameter 'lane' is missing.

None

Parameter 'file' has illegal value.

None

Plot Eye: Lane Name not found in the list of assigned physical lanes in Libero.Provide the correct lane name.

None

Parameter 'lane' has illegal value.

None

Parameter 'param_name' is not defined. Valid command formatting is 'plot_eye [-deviceName "device name"] -lane "Physical Lane Name" [-file "filename"] .

Supported Families

PolarFire
PolarFire SoC

Example

This example plots eye for lane {Q2_LANE0} and saves it into {./export.txt} file.

plot_eye -lane {Q2_LANE0} -file {./export.txt}