21.13.1.41 read_active_probe
(Ask a Question)Description
This Tcl command reads active probe values from the device. The target probe points are selected by the select_active_probe command.
When the user tries to read at least one signal from the bus/group, the complete bus or group is read. The user is presented with the latest value for all the signals in the bus/group.
read_active_probe [-deviceName device_name ] \
[-name probe_name ] \
[-group_name bus_name | group_name ] \
[-value_type b|h] \
[-file file_path ]
Arguments
Parameter | Type | Description |
---|---|---|
deviceName | string | Parameter is optional if only one device is available in the current configuration. |
name | string | Instead of all probes, read only the probes specified. The probe name should be prefixed with bus or group name if the probe is in the bus or group. |
group_name | string | Instead of all probes, reads only the specified buses or groups specified here. |
value_type | string | Optional parameter, used when the read value is stored into a variable as a string. b = binary h = hex |
file | string | Optional. If specified, redirects output with probe point values read from the device to the specified file. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'file' has illegal value. |
None | Parameter 'value_type' has illegal value. |
None | Parameter 'name' has illegal value. |
None | Parameter 'group_name' has illegal value. |
Supported Families
PolarFire |
PolarFire SoC |
SmartFusion 2 |
IGLOO 2 |
RTG4 |
Example
This example reads active probes of {group1}.
read_active_probe -group_name {group1}
See Also
select_active_probe
write_active_probe
delete_active_probe