21.13.1.56 save_live_probe_list
(Ask a Question)Description
This Tcl command saves the list of live probes to a file(*.txt).
save_live_probe_list [-deviceName "device name" -file "filename"
Arguments
Parameter | Type | Description |
---|---|---|
deviceName | string | Specify device name. This parameter is optional if only one device is available in the current configuration. |
file | string | Specify path and the name of output file(*.txt). This parameter is mandatory. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'file' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'save_live_probe_list [-deviceName "device name"] \ -file "filename"'. |
Supported Families
PolarFire |
PolarFire SoC |
SmartFusion 2 |
IGLOO 2 |
RTG4 |
Example
The following example saves live probes list to live_probe_list.txt file:
save_live_probe_list -file {./live_probe_list.txt}