21.13.1.67 signal_integrity_import
(Ask a Question)Description
This Tcl command imports Signal Integrity parameter options and other physical information for the selected lane/all lanes from an external PDC file.
signal_integrity_import -lane {phisical lane name} \
-pdc_file_name {path to the *.pdc file}
signal_integrity_import -all_lanes \
-pdc_file_name {path to the *.pdc file}
Arguments
Parameter | Type | Description |
---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
lane | string | Specifies the physical location of the lane. Must specify either '-lane' or '-all_lanes' command arguments. |
pdc_file_name | string | The path of the pdc file to be saved. |
all_lanes | none | Specifies all physical location of the lanes. Must specify either '-lane' or '-all_lanes' command arguments. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'param_name' is not defined. Valid command formatting is'signal_integrity_import [-deviceName "device name"] [-lane "Lane Instance Name"] [-all_lanes "TRUE | FALSE"] [-pdc_file_name "PDC File Name"]'. |
None | Signal Integrity: Must specify '-pdc_file_name. |
None | Signal Integrity: Import from *.pdc failed. Signal Integrity Constraints of lane not available in the file. |
None | Signal Integrity: Unable to Import from *.pdc file. |
None | Signal Integrity: Must specify one of '-lane'or '-all_lanes' command arguments. |
None | Signal Integrity: Must not specify both '-lane' and '-all_lanes' command arguments. |
None | Signal Integrity: Lane Name not found in the list of assigned physical lanes in Libero. Provide the correct lane name. |
Supported Families
PolarFire |
PolarFire SoC |
Example
The following example imports Signal Integrity parameter options and other physical information for the "Q0_LANE0" lane from ./SI_Q0LANE0.pdc:
signal_integrity_import -lane {Q0_LANE0} \
-pdc_file_name {./SI_Q0LANE0.pdc}
See Also
signal_integrity_export
signal_integrity_write
load_SI_design_defaults