21.13.1.66 signal_integrity_export
(Ask a Question)Description
This Tcl command exports the current selected parameter options and other physical information for the selected lane/all lanes instance to an external PDC file.
The exported content will be in the form of two "set_io" commands, one for the TXP port and one for the RXP port of the selected lane instance.
signal_integrity_export -lane {phisical lane name} \
-pdc_file_name {path to the *.pdc file}
signal_integrity_export -pdc_file_name {path to the *.pdc file} \
-all_lanes
Arguments
Parameter | Type | Description |
---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
lane | string | Specifies the physical location of the lane. You must specify either 'lane' or 'all_lanes' parameter. |
pdc_file_name | string | The path of the pdc file to be saved |
all_lanes | none | Specifies all physical location of the lanes. You must specify either 'lane' or 'all_lanes' parameter. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'param_names' is not defined. Valid command formatting is 'signal_integrity_export [-deviceName "device name"] [-lane "Lane Instance Name"] [-pdc_file_name "PDC File Name"] [-all_lanes "TRUE | FALSE"]'. |
None | Signal Integrity: Lane Name not found in the list of assigned physical lanes in Libero.Provide the correct lane name. |
None | Parameter 'pdc_file_name' has illegal value. |
None | Signal Integrity: Must not specify both '-lane' and '-all_lanes' command arguments. |
Supported Families
PolarFire |
PolarFire SoC |
Example
The following example exports the current selected parameter options and other physical information for the "Q0_LANE0" lane instance to an ./SI_Q0LANE0.pdc:
signal_integrity_export -lane {Q0_LANE0} \
-pdc_file_name {./SI_Q0LANE0.pdc}
See Also
signal_integrity_import
signal_integrity_write
load_SI_design_defaults