21.13.1.63 set_debug_programmer

Description

Identifies the programmer you want to use for debugging (if you have more than one).

set_debug_programmer -name { programmer_name }

Arguments

ParameterTypeDescription

name

string

Specify the programmer. This argument is mandatory.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Unable to select programmer 'prog_name' for debug.

None​

Required parameter 'name' is missing.

None​

Parameter 'param_name' is not defined. Valid command formatting is 'set_debug_programmer -name "programmer name"'

None​

Parameter 'name' has illegal value.

Supported Families

PolarFire
PolarFire SoC
SmartFusion 2
IGLOO 2
RTG4

Example

The following example selects the programmer 10841:

set_debug_programmer -name {10841}