21.13.1.62 set_debug_device
(Ask a Question)Description
Sets the device name in the tool.
set_debug_device -name “device name”
Arguments
Parameter | Type | Description |
---|---|---|
name | string | Specify the name of the device. This argument is mandatory. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'param_name' is not defined. Valid command formatting is 'set_debug_device -name "device name" |
None | Required parameter 'name' is missing. |
Supported Families
PolarFire |
PolarFire SoC |
SmartFusion 2 |
IGLOO 2 |
RTG4 |
Example
The following example sets MPF250T_ES as the device name:
set_debug_device -name “MPF250T_ES”