21.13.1.25 move_to_probe_group
(Ask a Question)Description
This Tcl command moves the specified probe points to the specified probe group.
Note:
Probe points related to a bus cannot be moved to another group.
move_to_probe_group -name {probe name} -group {group name}
Arguments
Parameter | Type | Description |
---|---|---|
name | string | Specifies one or more probes to move. |
group | string | Specifies name of the probe group. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'group' has illegal value. |
None | Required parameter 'group' is missing. |
None | Parameter 'name' has illegal value. |
None | Required parameter 'name' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is'move_to_probe_group [-name "name"]+ \-group "group name"'. |
Supported Families
PolarFire |
PolarFire SoC |
SmartFusion 2 |
IGLOO 2 |
RTG4 |
Example
This example moves {out[5]:out[5]:Q} and {grp1.out[3]:out[3]:Q} probes to the {my_grp2}:
move_to_probe_group -name {out[5]:out[5]:Q} \
-name {grp1.out[3]:out[3]:Q} \
-group {my_grp2}
See Also
create_probe_group
add_to_probe_group