21.13.1.58 select_active_probe

Description

This Tcl command manages the current selection of active probe points to be used by active probe READ operations. This command extends or replaces your current selection with the probe points found using the search pattern.

select_active_probe [–name probe_name_pattern ] \
                    [-reset true|false ]

Arguments

ParameterTypeDescription

name

string

Specifies the name of the probe. Optionally, search pattern string can specify one or multiple probe points. The pattern search characters “*” and “?” also can be specified to filter out the probe names.

reset

boolean

This optional parameter resets all previously selected probe points. If name is not specified, empties out current selection.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Parameter 'reset' has illegal value.

None

Parameter 'name' has illegal value.

None

Cannot select active probe: Specified probe point(s) not found.

None

Parameter 'param_name' is not defined. Valid command formatting is'select_active_probe [-name "name"]* \[-reset "TRUE | FALSE"]'.

Supported Families

PolarFire
PolarFire SoC
SmartFusion 2
IGLOO 2
RTG4

Example

Select_active_probe -name out[5]:out[5]:Q
Select_active_probe -name out.out[1]:out[1]:Q \
                    -name out.out[3]:out[3]:Q \
                    -name out.out[5]:out[5]:Q

See Also

  • write_active_probe

  • read_active_probe