21.13.1.52 remove_probe_insertion_point

Description

This Tcl command removes probe point from probe insertion list. The command will fail if the net name or driver are not specified or are incorrect.

Note:
  • Deleting probes from the probes list without clicking 'Run' does not automatically remove the probes from the design.

  • Probe Insertion feature disabled in the SmartDebug Demo and Standalone modes.

remove_probe_insertion_point -net {net_name} -driver {driver_name}

Arguments

ParameterTypeDescription

net

string

Specify name of the existing net which is added in probe insertion list. This parameter is mandatory.

driver

string

Specify driver name. This parameter is mandatory.

Return TypeDescription
NoneProbe insertion operations are not supported in Standalone SmartDebug.

Error Codes

Error CodeDescription

None

No probe point with net: "net_name" and driver: "driver_name" is added to be removed.

None

Parameter 'param_name' is not defined. Valid command formatting is 'remove_probe_insertion_point [-net "net_name"] [-driver "driver_name"] '.

Supported Families

PolarFire
PolarFire SoC
SmartFusion 2
IGLOO 2
RTG4

Example

The following example removes probe from the probe insertion list:

remove_probe_insertion_point -net {count_c[0]} -driver {Counter_out[0]:Q}

See Also

  • add_probe_insertion_point

  • program_probe_insertion