21.13.1.20 import_ddc_file
(Ask a Question)Description
This is a Standalone SmartDebug command. Enables you to import DDC file (created through Export SmartDebug Data in Libero) into the debug project.
import_ddc_file -import_ddc "DDC file" -device_name "device name"
Arguments
Parameter | Type | Description |
---|---|---|
import_ddc | string | Specify path to the DDC file. This parameter is mandatory. |
device_name | string | Specify the device name. This parameter is mandatory. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'import_ddc' is missing. |
None | Required parameter 'device_name' is missing. |
None | Failed to import DDC file '*.ddc'. There is no device 'device_name' in the current JTAG chain. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'import_ddc_file -import_ddc "DDC file" -device_name "device name"' |
Supported Families
PolarFire |
SmartFusion 2 |
IGLOO 2 |
RTG4 |
Example
This example importes DDC file to the debug project:
import_ddc_file -import_ddc {./src/top.ddc} -device_name {MPF250T_ES}
See Also
new_project