21.13.1.15 execute_dfe_calibration
(Ask a Question)Description
This Tcl command executes calibration. There are two types of calibration DFE (decision feedback equalizer) and CTLE (continuous time linear equalizer).
execute_dfe_calibration [-deviceName "device name"] \
-lane {physical location name} \
-full_calibration {0 | 1}
Arguments
Parameter | Type | Description |
---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
lane | string | Specify the physical lane instance name. |
full_calibration | boolean | This parameter specifies what kind of calibration you want to execute.
|
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Execute DFE Calibration: Lane Name not found in the list of assigned physical lanes in Libero.Provide the correct lane name |
None | Parameter 'lane' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is'execute_dfe_calibration [-deviceName "device name"] [-lane "Physical Lane Name"] [-full_calibration "TRUE | FALSE"]'. |
Supported Families
PolarFire |
PolarFire SoC |
Example
This example executes the dfe calibration for lane "Q0_Lane0".
execute_dfe_calibration -lane {Q0_Lane0} -full_calibration 1