21.13.1.53 rescan_programmer
(Ask a Question)Description
This Tcl command rescans for programmer connected to the host via the USB port.
Note:
This command does not have any arguments.
In the demo mode, this command returns "simulation".
rescan_programmer [-deviceName "device name"]
Arguments
Return Type | Description |
---|---|
String | Displays the programmer ID. |
Error Codes
Error Code | Description |
---|---|
None | No programmers found. Check the programmer connection to the computer and ensure the drivers are properly installed. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'rescan_programmer [-deviceName "device name"] '. |
Supported Families
PolarFire |
PolarFire SoC |
SmartFusion 2 |
IGLOO 2 |
RTG4 |
Example
This example rescans the programmer connection.
rescan_programmer
This example rescans and retrieves the programmer name.
set programmer_id [rescan_programmer]
puts $programmer_id