Description
Returns
details about all of the clock constraints in the
current timing constraint scenario.
list_clocks
Arguments
Parameter | Type | Description |
---|
None | None | None |
Return Type | Description |
---|
string | Returns details about all of the clock constraints in the current timing constraint scenario. |
Supported
Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Example
The following example displays the details about all of the clock constraints in the current timing constraint scenario.
puts [list_clocks]
Related Examples on GitHub