21.8.23 list_generated_clocks
(Ask a Question)Description
Returns details about all of the generated clock constraints in the current timing constraint scenario.
list_generated_clocks
Arguments
Return Type | Description |
---|---|
string | Returns details about all of the generated clock constraints in the current timing constraint scenario. |
Supported Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Example
The following example displays the details about all of the generated clock constraints in the current timing constraint scenario.
puts [list_generated_clocks]