21.8.39 remove_false_path
(Ask a Question)Description
Removes
a false path constraint from the current timing scenario by specifying either its
exact arguments or its ID. If the arguments do not match a false path constraint in
the current scenario, or if the specified ID does not refer to a false path
constraint, this command fails.
Note: Do not specify both false path arguments and the constraint ID.
remove_false_path [-from from_list] [-to to_list] [-through through_list] | -id constraint_ID
Arguments
Parameter | Type | Description |
---|---|---|
from | list of strings | Specifies a list of timing path starting points. A valid timing starting point is a clock, a primary input, an inout port, or a clock pin of a sequential cell. |
through | list of strings | Specifies a list of pins, ports, nets, or instances (cells) through which the disabled paths must pass. |
to | list of strings | Specifies a list of timing path ending points. A valid timing ending point is a clock, a primary output, an inout port, or a data pin of a sequential cell. |
id | integer | Specifies the ID of the false path constraint to remove from the current scenario. You must specify either the exact false path arguments to remove or the constraint ID that refers to the false path constraint to remove. |
Error Codes
Error Code | Description |
---|---|
None | Invalid arguments -from/-to/-through. |
None | Only one argument is needed. |
Supported Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Exceptions
You cannot use wildcards when specifying a clock name, either alone or in an accessor command
such as get_pins
or get_ports
.
Example
The following example specifies all false path to remove.
remove_false_path -through U0/U1:Y
The following example removes the false path constraint using its id.
set fpId [set_false_path -from [get_clocks c*] -through {topx/reg/*} \
-to [get_ports out15] ]
remove_false_path -id $fpId