21.8.25 list_max_delays
(Ask a Question)Description
Returns details about all of the maximum delay constraints in the current timing constraint scenario.
list_max_delays
Arguments
Return Type | Description |
---|---|
string | Details about all of the max delay constraints in the current timing constraint scenario. |
Supported Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Example
With this command we get the details about all of the maximum delay constraints in the current timing constraint scenario.
puts [list_max_delays]