21.8.55 set_current_scenario
(Ask a Question)Description
Specifies the timing scenario for the Timing Analyzer to use. All commands that follow this command will apply to the specified timing scenario. A timing scenario is a set of timing constraints used with a design. If the specified scenario is already the current one, this command has no effect.
After setting the current scenario, constraints can be listed, added, or removed, the checker can be invoked on the set of constraints, and so on.
This command uses the specified timing scenario to compute timing analysis.
Note: It is recommended to use the
organize_tool_files command instead of this command.
set_current_scenario name
Arguments
Parameter | Type | Description |
---|---|---|
name | string | Specifies the name of the timing scenario to which to apply all commands from this point on. |
Supported Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Example
The following command sets scenario_A
as current scenario of the timing
scenario.
set_current_scenario scenario_A