21.8.46 remove_scenario
(Ask a Question)Description
Removes a scenario from the constraint database and removes it to the list of scenarios.
remove_scenario name
Arguments
Parameter | Type | Description |
---|---|---|
name | string | Specifies the name of the scenario to delete. This is mandatory. |
Error Codes
Error Code | Description |
---|---|
None | Required parameter _AtclParam0_ is missing. |
Supported Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Exceptions
You cannot use wildcards when specifying a set name to remove.
Example
The following command removes the scenario named my_scenario
.
remove_scenario my_scenario