21.8.21 list_disable_timings
(Ask a Question)Description
Returns the list of disable timing constraints for the current scenario.
list_disable_timings
Arguments
Return Type | Description |
---|---|
string | Returns list of disable timing constraints for the current timing constraint scenario. |
Supported Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Example
With this command we get the disable timing constraints in the current timing constraint scenario.
puts [list_disable_timings]