21.8.24 list_input_delays
(Ask a Question)Description
Returns details about all of the input delay constraints in the current timing constraint scenario.
list_input_delays
Arguments
Return Type | Description |
---|---|
string | Details about all of the input delay constraints in the current timing constraint scenario. |
Supported Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Example
With this command we get the details about all of the input delay constraints in the current timing constraint scenario.
puts [list_input_delays]