21.3.97 unset_as_target

Description

This Tcl command unsets a target file in the Constraints view to not to store constraints. To unset *.sdc *.pdc files as target, click the Manage Constraints tool name from Design Flow.

unset_as_target -file { absolute path to file }

Arguments

ParameterTypeDescription
filestringSpecifies the absolute path to file to be unset as a target.

Error Codes

Error Code

Description

None

Parameter 'param_name' is not defined. Valid command formatting is 'unset_as_target -file "file to unset as target"'.

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

This command unsets the SDC file <project_folder>/constraint/user.sdc as target to not store SDC command.

unset_as_target -file {/prj_path/constraint/user.sdc}

See Also