21.3.76 rename_file

Description

This Tcl command copies/renames a file specified by the -file parameter to a different name specified by the -target parameter. Creates a new file in the <project_name> directory.

rename_file -file { absolute path and the name of file } -target { new_filename }

Arguments

ParameterTypeDescription
filestringSpecifies the absolute path and original name of the file.
targetstringSpecifies the just new name of the file. If specified constraint file, then created new file in constraint directory, otherwise new file created in the <project_name> directory, not renamed.

Error Codes

Error CodeDescription
NoneRequired parameter 'file' is missing.
NoneParameter 'file' has illegal value.
NoneRequired parameter 'target' is missing.

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following command copies the constraint a.sdc file specified by the -file parameter to a b.sdc specified by -target parameter in the "c:/user/" directory.

rename_file -file {c:/user/a.sdc} -target {b.sdc}

The following command copies the a.v verilog file specified by the -file parameter to a b.v specified by -target parameter in the project directory not in hdl.

rename_file -file { /libero_prj/hdl/a.v } -target {b.v}