21.3.30 export_as_link

Description

This Tcl command exports a file to another directory and links to the file.

export_as_link -file {absoulte or relative path and name of the file} \
               -path link_path

Arguments

ParameterTypeDescription
filestringSpecifies absolute or relative path and name of the file you want to export as a link.
pathstringPath of the link.

Error Codes

Error CodeDescription
None'c.v' must not be part of a component and must be local to the project.

None

Required parameter 'file' is missing.

None

Parameter 'file' has illegal value.

None

Required parameter 'path' is missing.

None

Parameter 'param_name' is not defined. Valid command formatting is 'export_as_link -file "file" -path "link path" '.

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

Export the file hdl1.vhd as a link to c:\Microchip\link_source.

export_as_link -file hdl1.vhd -path {c:\Microchip\link_source}