21.3.59 import_files

Description

This Tcl command enables you to import design source files and constraint files.

For importing constraint files, import_files has retired the -pdc parameter for SmartFusion 2, IGLOO 2, PolarFire and RTG4. It has been replaced with two new parameters to match the new design flow. Physical Design Constraints (PDC) Tcl must now be divided between I/O attribute and pin information from all floorplanning and timing constraints. These commands must now reside in and be imported as separate files. The new parameters specify the type of *.pdc file being imported. The path to the file can be absolute or relative but must be enclosed in curly braces { }.

Use the -convert_EDN_to_HDL parameter to convert the EDIF file to HDL and then import the converted HDL file.

Note: The EDIF File is not imported.
import_files \
-schematic {file} \
-symbol {file} \
-smartgen_core {file} \
-ccp {file} \
-stimulus {file} \
-hdl_source {file} \
-io_pdc {file} \
-fp_pdc {file} \
-edif {file} \
-sdc {file} \
-crt {file} \
-dcf {file} \
-vcd {file} \
-saif {file} \
-simulation {file} \
-profiles {file} \
-cxf {file} \
-templates {file} \
-ccz {file} \
-modelsim_ini {file} \
-library {file} \
-convert_EDN_to_HDL {true | false}

Arguments

ParameterTypeDescription
schematicstringSpecifies the schematics you wish to import into your IDE project. Type parameter must be repeated for each file.
symbolstringSpecifies the symbols you wish to import into your IDE project. Type parameter must be repeated for each file.
smartgen_corestringSpecifies the SmartGen Cores you wish to import into your project. Type parameter must be repeated for each file.
ccpstringSpecifies the Arm® or Cortex®-M1 cores you wish to import into your project. Type parameter must be repeated for each file.
stimulusstringSpecifies HDL stimulus files you wish to import into your project. Type parameter must be repeated for each file.
hdl_source_folderstringName of the HDL folder you want to import into your project.
hdl_sourcestringSpecifies the HDL source files you wish to import into your project. Type parameter must be repeated for each file.
io_pdcstringSpecifies the PDC file that contains the I/O attribute and pin information.
fp_pdcstringSpecifies the PDC file that contains the timing and placement information.
edifstringSpecifies the EDIF files you wish to import into your project. Type parameter must be repeated for each file. This is a mandatory option if you want to convert EDIF to HDL with the -convert_EDN_to_HDL option. This option is not supported in PolarFire.
sdcstringSpecifies the SDC constraint files you wish to import into your project. Type parameter must be repeated for each file.
crtstringSpecifies the CRT constraint files you wish to import into your project. Type parameter must be repeated for each file. This option is not supported for PolarFire®, SmartFusion® 2, IGLOO® 2, and RTG4™ families.
dcfstringSpecifies the DCF constraint files you wish to import into your project. Type parameter must be repeated for each file.
Note: Not supported for PolarFire, SmartFusion 2, IGLOO 2, and RTG4 families.
vcdstringSpecifies the VCD constraint files you wish to import into your project. Type parameter must be repeated for each file.
saifstringSpecifies the SAIF constraint files you wish to import into your project. Type parameter must be repeated for each file.
simulationstringSpecifies the simulation files you wish to import into your Libero SoC project. Type parameter must be repeated for each file.
profilesstringSpecifies the profile files you wish to import into your Libero SoC project. Type parameter must be repeated for each file.
cxfstringSpecifies the CXF (Component) file you wish to import into your Libero SoC project. Type parameter must be repeated for each file.
templatesstringSpecifies the template file you wish to import into your project.
cczstringSpecifies the IP Control core file you wish to import into your project.
modelsim_inistringSpecifies the ModelSIM INI file that you wish to import into your project.
librarystringSpecifies the library file that you wish to import into your project. If a library file is not available it will be created and added to the library.
convert_EDN_to_HDLbooleanThe -edif option is mandatory. If the –edif option is not specified or the -convert_EDN_to_HDL is used with another option, EDIF to HDL conversion will fail.

Error Codes

Error CodeDescription
NoneUnable to find the file 'a.v'.
NoneCannot import the 'ProASIC Constraint Files'; your selected family does not support GCF constraints.
NoneCannot import the 'Criticality Files'; your selected family does not support CRT constraints.
NoneCannot import the 'Timing Constraint Files'; your selected family does not support DCF constraints.
NoneCannot import the 'Pin Files'; your selected family does not support PIN constraints.
NoneError: Parameter is not defined. Valid command formatting is 'import_files [-convert_EDN_to_HDL "TRUE | FALSE"] \ [-hdl_source_folder "Source folder"]* \ [-library "library"] \ [-cxz "file"]* \ [-cxf "file"]* \ [-ccp "file"]* \ [-crt "file"]* \ [-hdl_source "file"]* \ [-stimulus "file"]* \ [-templates "file"]* \ [-modelsim_ini "file"]* \ [-fp_pdc "file"]* \ [-io_pdc "file"]* \ [-sdc "file"]* \ [-ndc "file"]* \ [-net_fdc "file"]* \ [-icf "file"]* \ [-ccz "file"]* \ [-cpz "file"]* \ [-pin "file"]* \ [-gcf "file"]* \ [-saif "file"]* \ [-schematic "file"]* \ [-simulation "file"]* \ [-smartgen_core "file"]* \ [-symbol "file"]* \ [-verilog_netlist "file"]* \ [-dcf "file"]* \ [-profiles "file"]* \ [-vcd "file"]*

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The command below imports the HDL source files file1.vhd and file2.vhd.

import_files -hdl_source file1.vhd –hdl_source file2.vhd