21.3.48 export_sdc_file

Description

This Tcl command exports the file for timing constraints. The exported file has a *.sdc file name extension.

export_sdc_file -file { absolute path and name of *.sdc file }

Arguments

ParameterTypeDescription
filestringSpecifies the SDC file to export.

Error Codes

Error Code

Description

None

Required parameter 'file' is missing.

None

Parameter 'param_name' is not defined. Valid command formatting is 'export_sdc_file -file "Export SDC File Name"' .

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following command exports the SDC file for timing constraints to sd1.sdc.

export_sdc_file -file {E:/designs/export/sd1.sdc}