21.3.49 export_smart_debug_data

Description

This Tcl command exports debug data for the SmartDebug application and creates *.ddc that contains data based on selected options. The command corresponds to the Export SmartDebug Data tool in Libero. This file is used by SmartDebug (standalone application) to create a new SmartDebug project, or it can be imported into a device in SmartDebug (standalone application).

Important:
  • If you do not specify any design components, all components available in the design will be included by default except the bitstream components.

  • The generate_bitstream parameter is required if you want to generate bitstream file and include it in the exported file.

  • You must specify the bitstream components you want to include in the generated bitstream file or all available components will be included.

  • If you choose to include bitstream, and the design has custom security, the custom security bitstream component must be included.

export_smart_debug_data [-file_name "file_name"] \ [-export_dir "export_dir"] \ [-probes "TRUE | FALSE"] \ [-package_pins "TRUE | FALSE"] \ [-memory_blocks "TRUE | FALSE"] \ [-envm_data "TRUE | FALSE"] \ [-security_data "TRUE | FALSE"] \ [-display_security_in_smartdebug "TRUE | FALSE"]\ [-chain "TRUE | FALSE"] \ [-programmer_settings "TRUE | FALSE"] \ [-ios_states "TRUE | FALSE"] \ [-generate_bitstream "TRUE | FALSE"] \ [-bitstream_format "PPD | STP"] \ [-bitstream_security "TRUE | FALSE"] \ [-bitstream_fabric "TRUE | FALSE"] \ [-bitstream_envm "TRUE | FALSE"] \ [-bitstream_snvm "TRUE | FALSE"] \ [-snvm_data "TRUE | FALSE"] \ [-sanitize_snvm "TRUE | FALSE" ] \ [-sanitize_envm "TRUE | FALSE" ] \ [-master_include_plaintext_passkey "TRUE|FALSE"]\ [-uprom_data "TRUE | FALSE"] \ [dpk_security "TRUE | FALSE"] \ [upk1_security "TRUE | FALSE"]

Arguments

ParameterTypeDescription

file_name

string

Name of the exported file with extension .ddc.

export_dir

string

Location where the DDC file will be exported. If omitted, the design export folder will be used.

probes

boolean

Specified probes related data to be included in the DDC file, data used for Active/Live

package_pins

boolean

Specifes probe insertion related data to be included in the DDC file.

memory_blocks

boolean

Specifes memory blocks such as LSRAM and USRAM related data to be included in DDC file.

security_data

boolean

Specifies security keys related data.

display_security_in_smartdebug

boolean

If security_data is set to 1, then this option is included to hide/show passkeys on SmartDebug main window option provided in 12.4 release.

chain

boolean

This option is set if user wants to connect the devices in chain.

programmer_settings

boolean

Programmer related settings from Libero to be included in DDC file.

io_states

boolean

I/O states information preserved during programming to be included in DDC file.

snvm_data

boolean

Set to 1 if snvm debug related information needs to be included in the DDC file.
Note: This parameter is only applicable to PolarFire, PolarFire SoC and RT PolarFire devices.

envm_data

boolean

Set to 1 if envm debug related information needs to be included in DDC file. Applicable to PF SOC device only. Option provided from 12.5 release onwards.

generate_bitstream

boolean

Bitstream content to be included in the DDC file.

bitstream_format

string

Bitstream generated format option. The valid values are: PPD, STAPL.

bitstream_security

boolean

Bitstream security pass keys information needed in bitstream to be included along with bitstream.

master_include_plaintext_passkey

boolean

This option indicates whether plaintext passkey needs to be included for REPROGRAM/ERASE action in SASD.

bitstream_fabric

boolean

Bitstream fabric component included in bitstream.

bitstream_snvm

boolean

If snvm component needs to be included in the bitstream. Applicable to PF, PFSOC, RTPF family only.

bitstream_envm

boolean

If envm component needs to be included in the bitstream. Applicable to SF2, PFSOC family only.

sanitize_snvm

boolean

If snvm has to be sanitized during ERASE action. Applicable to PF, PFSOC only, providede in 2021.2 release.

sanitize_envm

boolean

If envm has to be sanitized during ERASE action. Applicable to PFSOC only, provided in 2021.2 release.

dpk_securitybooleanSpecifies to include the debug pass key security information for debug.
upk1_securitybooleanSpecifies to include the User Passcode Key 1 security information for debug.
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

probes: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

package_pins: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

memory_blocks: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

security_data: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

chain: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

programmer_settings: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

ios_states: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

generate_bitstream: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

bitstream_security: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

bitstream_fabric: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

bitstream_snvm: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0, or false).

None

Parameter 'param_names' is not defined. Valid command formatting is'export_smart_debug_data [-file_name "file_name"] \[-export_dir "export_dir"] \[-probes "TRUE | FALSE"] \[-package_pins "TRUE | FALSE"] \[-memory_blocks "TRUE | FALSE"] \[-envm_data "TRUE | FALSE"] \[-security_data "TRUE | FALSE"] \[-display_security_in_smartdebug "TRUE | FALSE"] \[-chain "TRUE | FALSE"] \[-programmer_settings "TRUE | FALSE"] \[-ios_states "TRUE | FALSE"] \[-generate_bitstream "TRUE | FALSE"] \[-bitstream_format "PPD | STP"] \[-bitstream_security "TRUE | FALSE"] \[-bitstream_fabric "TRUE | FALSE"] \[-bitstream_envm "TRUE | FALSE"] \[-bitstream_snvm "TRUE | FALSE"] \[-master_include_plaintext_passkey "TRUE | FALSE"] \[-uprom_data "TRUE | FALSE"] \[-snvm_data "TRUE | FALSE"]'.

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following examples show the export_smart_debug_data command with all parameters.

SmartFusion 2, IGLOO 2, RTG4 example:

export_smart_debug_data \ -file_name {sd1} \ -export_dir {d:\sd_prj\test3T\designer\sd1\export} \ -force_rtg4_otp 1 \ -probes 1 \ -package_pins 0 \ -memory_blocks 1 \ -envm_data 0 \ -security_data 1 \ -chain 1 \ -programmer_settings 1 \ -ios_states 1 \ -generate_bitstream 0 \ -bitstream_security 0 \ -bitstream_fabric 0 \ -bitstream_envm 0

PolarFire examples:

export_smart_debug_data \ -file_name "top" \ -export_dir."/" \ -probes 1 \ -package_pins 0 \ -memory_blocks 1 \ -security_data 1 \ -chain 1 \ -programmer_settings 1 \ -ios_states 1 \ -generate_bitstream 1 \ -bitstream_security 0 \ -bitstream_fabric 1 \ -bitstream_snvm 1
​​​export_smart_debug_data \ -file_name {smartdebug_export.ddc} \ -export_dir{H:\Designs\mss\designer\sd\export} \ -probes 1 \ -package_pins 0 \ -memory_blocks 1 \ -envm_data 1 \ -security_data 1 \ -display_security_in_smartdebug 0 \ -chain 1 \ -programmer_settings 1 \ -ios_states 1 \ -generate_bitstream 1 \ -bitstream_format {PPD} \ -bitstream_security 0 \ -bitstream_fabric 1 \ -bitstream_envm 1 \ -sanitize_envm 1 \ -bitstream_snvm 1 \ -sanitize_snvm 1 \ -master_include_plaintext_passkey 0 \ -snvm_data 1