21.3.40 export_io_pdc

Description

This Tcl command exports the I/O Physical Design Constraint (*.pdc) File. You can export the I/O PDC file from Constraint Manager > I/O Attributes or Constraint Manager Floor Planner or from File menu. Constraints can be exported to PDC file for reference, but must be manually added to an existing PDC or imported via the Constraints Editor for the changes to affect the final paced and routed design. The exported file has *.pdc file name extension. Before exporting, you need to run 'Place and Route'.

export_io_pdc -file { absolute or relative path and name of *.pdc file }

Arguments

ParameterTypeDescription
filestringSpecifies absolute or relative path and name of the *.pdc file. It is mandatory. There may be multiple -file arguments (see example below).

Error Codes

Error CodeDescription
NoneRequired parameter 'file' is missing.

None

Parameter 'param_name' is not defined. Valid command formatting is 'export_io_pdc -file "Export IO PDC File Name" '.

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following example exports information about all of the physical design constraints (I/O constraints, I/O Banks, routing constraints, region constraints, global and local clocks). Created both "sd_io1.pdc" and "sd_io2.pdc" files.

export_io_pdc -file {./sd_io1.pdc} -file {sd_io2.pdc}

See Also