21.3.54 get_libero_version

Description

This Tcl command returns the version number of the Libero SoC version. The value that is returned is the same as the version number that is displayed in the Help > About Libero window.

get_libero_version

Arguments

Return TypeDescription
stringReturns the version number of the Libero SoC version.

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following example displays Libero version number with var2 variable.

get_libero_version
#save into a variable
set var2 [get_libero_version]
#display variable
puts "Libero Version is $var2"

You will see output similar to the following.

Libero Version is 12.6.0

See Also