21.3.7 change_link

Description

This Tcl command changes the source of a linked file in your project.

change_link -file filename -path new_source_path

Arguments

ParameterTypeDescription
filestringSpecifies absolute or relative path and name of the linked file you want to change.
pathstringLocation of the file (absolute or relative path) you want to link to.

Error Codes

Error Code

Description

None

Required parameter 'path' is missing.

None

Required parameter 'file' is missing.

None

Parameter 'file' has illegal value.

None

Parameter 'param_name' is not defined. Valid command formatting is 'change_link -file "file" -path "new source path"'

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

  1. Change the link to a file 'sim1.vhd' in your project and link it to the c:\Microchip\link_source\simulation_test.vhd file.
    change_link -file sim1.vhd \
                -path {c:\Microchip\link_source\simulation_test.vhd}
  2. Change link for the file 'test.v' from 'E:\Share\test.v' to 'E:\Share\test\srcs\test.v' using environment variable 'MSCC_ROOT_1' that has the root directory path 'E:\Share'.
    change_link -file {${MSCC_ROOT_1}/test.v} \
                -path {${MSCC_ROOT_1}/test/srcs/test.v}

See Also