21.3.87 set_device

Description

This Tcl command sets your device family, die, and package in the Project Manager. This command generates the set_device.log file that contains information on device details. The file is saved in the <project_name>/tooldata folder.

Important: The changes you make may invalidate your components and/or design flow; you may have to regenerate your components and rerun your design flow.
set_device [-family "family" ] [-die "die" ] [-die_voltage "value" ] \
           [-part_range "part_range" ] [-package "package" ] \
           [-speed "speed_grade" ] [-adv_options "value" ]

Arguments

ParameterTypeDescription
familystringSets device family. If you have already set device name, you cannot change the device family name for the current project; however, you can change the rest of the arguments.
diestringSets device die. It is optional.
die_voltagefloating pointSets the die voltage for your project. Possible values depend on your device. For more details, see the device datasheet.
part_rangestringSets the default temperature range for your project:
  • PolarFire®: EXT, IND, and MIL
  • SmartFusion® 2: COM, IND, TGrade 2, and MIL
  • IGLOO® 2: COM, IND, TGrade 1, TGrade 2, and MIL
  • RTG4™: MIL
packagestringSets device package. It is optional.
speedstringSets device speed grade. Valid values: -1 and STD. It is optional.
adv_optionsstringSets the advanced options, such as temperature and voltage settings.
  • IO_DEFT_STD:LVTTL - Sets the I/O default value to LVTTL.
  • TEMPR:COM - Sets the default temperature range; can be COM (Commercial), MIL (Military), or IND (industrial).
  • VCCI_1.5_VOLTR:COM - Sets VCCI to 1.5 and voltage range to Commercial.
  • VCCI_1.8_VOLTR:COM - Sets VCCI to 1.8 and voltage range to Commercial.
  • VCCI_2.5_VOLTR:COM - Sets VCCI to 2.5 and voltage range to Commercial.
  • VCCI_3.3_VOLTR:COM - Sets VCCI to 3.3 and voltage range to Commercial.
  • VOLTR:COM - Sets the voltage range; can be COM (Commercial), MIL (Military), or IND (industrial).
  • RESTRICTPROBEPINS:1 - Sets to 1 to reserve pins for probing if you intend to debug using SmartDebug.
  • RAD_EXPOSURE: <value> - Specifies the radiation exposure in Krad. Supported on RTG4 devices, as well as RTPF and RTPFS device part numbers within PolarFire and PolarFire SoC families, respectively. Valid range:
    • RTG4: Integer between 0 and 100
    • RTPF and RTPFS: Either 0 or 100

    For RT PolarFire devices, such as RTPF500ZTL, specify the device using ‘-family {PolarFire}’ and set the radiation exposure using -adv_options {RAD_EXPOSURE:100}.

  • SYSTEM_CONTROLLER_SUSPEND_MODE: Enables or disables the System Controller Suspend mode.

You can provide custom temperature ranges depending on the selected part range.

The value parameter needs minimum, typical, and maximum temperature values to be added. The following table denotes the minimum, typical, and maximum temperatures that are preset by the tool. You can set any value for the temperatures present within the range.

Part RangeMinimumTypicalMaximum
EXT025100
COM (Available only for SmartFusion® 2 and IGLOO® 2 devices)02585
IND-4025100
MIL-5525125

Error Codes

Error CodeDescription
NoneUnable to select speed 'ALL'. The speed value must be '-1 STD'.

None

Unable to select family 'value'. The family value must be one of the following: 'IGLOO® 2', 'SmartFusion® 2', 'RTG4™', 'PolarFire®', or 'PolarFire SoC'.

None

Unable to select die 'MPF0T'. The die value must be one of the following: 'MPF300T_ES', 'MPF300TS_ES', 'MPF050T', 'MPF050TS', 'MPF100T', 'MPF100TS', 'MPF200T', 'MPF200TS', 'MPF300T', 'MPF300TS', 'MPF500T', 'MPF500TS', 'MPF300XT', 'MPF050TL', 'MPF100TL', 'MPF200TL', 'MPF300TL', 'MPF500TL', 'MPF050TLS', 'MPF100TLS', 'MPF200TLS', 'MPF300TLS', 'MPF500TLS', 'RTPF500T', 'RTPF500TL', 'RTPF500TS', 'RTPF500ZTL', or 'RTPF500TLS'.

NoneInvalid value "TGrade2" for PART_RANGE variable; expected one of COM IND.
NoneInvalid value "MIL" for VCCI_1.2_VOLTR variable; expected one of COM IND.

None

No family was specified. Select a family before proceeding.

None

Parameter 'param_name' is not defined. Valid command formatting is 'set_device [-family "family"] [-die "die"] [-package "package"] [-speed "speed"] [-die_voltage "die_voltage"] [-part_range "part_range"] [-adv_options "adv_options"].

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following command sets the SmartFusion 2 family with M25005 die, 484 FBGA package, {-1} speed, IND part range, temperature, and voltage settings to your device.

set_device -family {SmartFusion 2} \
-die {M2S005} \
-package {484 FBGA} \
-speed {-1} \
-die_voltage {1.2} \
-part_range {IND} \
-adv_options {IO_DEFT_STD:LVCMOS 2.5V} \
-adv_options {RESERVEMIGRATIONPINS:1} \
-adv_options {VCCI_2.5_VOLTR:COM} \
-adv_options {VCCI_3.3_VOLTR:COM} \
-adv_options {VOLTR:IND}\
-adv_options {SYSTEM_CONTROLLER_SUSPEND_MODE:1}

The following command sets the RTG4 family with RTG4150 die, 1657_CG package, {STD} speed, MIL part range, and a custom temperature range: minimum = 0, typical = 25, and maximum = 70.

set_device -family {RTG4} -die {RTG4150} -package {1657_CG} -speed {STD} -die_voltage {1.2} -part_range {MIL} -adv_options  {TEMPR:0 25 70} -adv_options {SYSTEM_CONTROLLER_SUSPEND_MODE:1}

The following command sets the PolarFire family with MPF200T die, FCG784 package, {-1} speed, EXT part range, and a custom temperature range: minimum = 0, typical = 25, and maximum = 70.

set_device -family {PolarFire} -die {MPF200T} -package {FCG784} -speed {-1} -part_range {EXT} -adv_options  {TEMPR:0 25 70} -adv_options {SYSTEM_CONTROLLER_SUSPEND_MODE:1}
The following command sets an RT PolarFire device using the PolarFire family, with radiation exposure set to 100 Krad.
set_device -family {PolarFire} \
-die {RTPF500ZTL} \
-package {FC1509} \
-speed {STD} \
-die_voltage {1.0} \
-part_range {MIL} \
-adv_options {IO_DEFT_STD:LVCMOS 1.8V} \
-adv_options {RAD_EXPOSURE:100}