21.3.85 set_active_testbench

Description

This Tcl command sets the active testbench module to be executed during the simulation process.
Important: To specify a custom list of stimulus files needed for the simulation, use the associate_stimulus command.
set_active_testbench "<testbench_name>::<library_name>,<file_path>"

Error Codes

Error CodeDescription
NoneNone

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

Example 1: This example instructs the tool to use the tb1 module from the work library and specifies the location of the source file (stimulus/tb1.v).

set_active_testbench "tb1::work,stimulus/tb1.v"

Example 2: This example instructs the tool to use the sdtb1 SmartDesign testbench module from the work library and specifies the location of the source file (component/work/sdtb1/sdtb1.v).

set_active_testbench "sdtb1::work,component/work/sdtb1/sdtb1.v"