21.3.64 open_project

Description

This Tcl command opens an existing Libero SoC project. You can create backup of your original project before opening.

open_project -file "project file" \
             [-do_backup_on_convert "TRUE | FALSE"] \
             [-backup_file "backup archive file name"]

Arguments

ParameterTypeDescription
filestringMust include the complete path to the PRJ file. If you do not provide the full path, Libero SoC infers that you want to open the project from your current working directory.
do_backup_on_convert

boolean

Sets the option to backup your files if you open a project created in a previous version of Libero SoC.
  • TRUE - creates a backup of your original project before opening.
  • FALSE - opens your project without creating a backup.
backup_filestringSets the name of your backup file (if you choose to do_backup_on_convert).

Error Codes

Error CodeDescription
NoneUnable to find project file: /exprj/exprj.prjx.

None

Required parameter 'file' is missing.

None

Parameter 'backup_file' has illegal value.

None

Parameter 'backup_file' : the file '/prj_path/archive' has got an invalid extension. Valid extension is 'zip'.

None

do_backup_on_convert: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0 or false).

None

Parameter 'param_name' is not defined. Valid command formatting is 'open_project -file "project file" [-do_backup_on_convert "TRUE | FALSE"] [-backup_file "backup archive file name"] ' .

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following command opens project.prjx project from test directory without creating a backup file.

open_project -file {c:/netlists/test/project.prjx}

See Also