21.3.45 export_profiles

Description

This Tcl command exports your tool profiles. Performs the same action as the Export Profiles dialog box.

export_profiles -file { absolute path and name of exported file } \
                [-export "value" ]

Arguments

ParameterTypeDescription
filestringSpecifies the absolute path and name to the exported profile file.
exportstringSpecifies your profile export options. The following table shows the acceptable values for this argument:
  • predefined - exports only predefined profiles
  • user - exports only user profiles
  • all - exports all profiles

Error Codes

Error CodeDescription
NoneParameter 'file' : the file '/prj/profiles_command/exp.tcl' has got an invalid extension. Valid extension is 'ini'.

None

Required parameter 'file' is missing.

None

Parameter 'file' has illegal value.

None

Parameter 'param_name' is not defined. Valid command formatting is 'export_profiles -file "file name" [-export "predefined | user | all"] '.

Supported Families

Supported Families
PolarFire®
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following command exports all profiles to the file './profile_commands/all_profiles'.

export_profiles -file "./profile_commands/all_profiles" -export all

See Also